FSYNC Y-Adapter
Based on
RVC
Dot projector
No
Infrared
No
IMU
None

Looking for more details? Visit specific features at Platform -> Features
Overview
- All Series 2 OAK POE cameras: OAK-D S2 PoE, OAK-D W PoE, OAK-D Pro PoE, OAK-D Pro W PoE. These currently require an external FSYNC signal (see the relevant part of the docs below)
- OAK-D ToF - follow the Getting Started below
- OAK Thermal - follow the Getting Started below
Getting Started
OAK-D-SR-POE that doesn't have a cable connected to "IN" port (M8 female connector) will output FSYNC signal automatically and will therefore be the "FSYNC Host" device, while devices that have a cable connected to "IN" port will be "FSYNC Peripheral" devices.FSYNC results
Auto-Exposure, TS difference is a bit larger (13ms), as color sensors have ~25ms longer exposure time (and we take middle of exposure, so /2):
Hardware syncing 4x OAK PoE cameras. Manual exposure of 6ms for color cameras, 1ms mono cameras:
Script used can be found here. We used External FSYNC signal (see below) in this case, as we tested it with 2x OAK-D Pro PoE cameras. The mobile phone screen was set to 120 Hz refresh rate.External FSYNC signal
Wiring diagram
Photo of the wiring
BNC to M8 adapter
Wiring diagram

Python
1# One needs to set the FSYNC mode to INPUT to all camera's sensors:
2cam1 = pipeline.create(dai.node.MonoCamera)
3cam1.initialControl.setFrameSyncMode(dai.CameraControl.FrameSyncMode.INPUT)
4
5cam2 = pipeline.create(dai.node.ColorCamera)
6cam2.initialControl.setFrameSyncMode(dai.CameraControl.FrameSyncMode.INPUT)
7# ...Dimensions and Weight
- Weight: 5g
- Width: 23.5 mm
- Height: 33 mm
- Length: 10 mm